Content originally posted in LPCWare by pra18 on Thu Jul 31 08:43:49 MST 2014
Hi,
I have a question w.r.t the DFU usng USB on lpc43xx.
Do we need to use the USB boot mode only if we have a DFU USB implementation in place on my device ?
OR
Do we need to use the USB boot mode only if we have a CDC USB implementation in place on my device ?
I have seen in a ARM9 product that if there is a CDC USB acting as a VirtualCOM one can boot
using the USB but with a precondition that there should be a USB cable connected at power up.
suppose that I have already Serial flash and USART3 boot modes enabled on my platform and I need a USB0 or USB1
boot mode in addition, do I need some special method to achieve booting through USB?
Please consider that I dont intend to implement a DFU but would have a CDC USB rather.
What if I would have a CDC class USB in my firmware and will I have to then support USB boot mode in HW.
Thanks in advance,