LPC43xx USB isochronous mode & windows driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC43xx USB isochronous mode & windows driver

470 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RichardsonM on Fri Jul 06 04:02:13 MST 2012
Hi,

I'm looking at using an LPC43xx device with the USB port running in isochrounous mode using nxpUSBlib for a high speed custom data interface (up to around 150Mbps). Is this possible and do you know if there's a windows driver that I can use from a custom windows application to access the data sent from the LPC43xx?

Thanks for any help you can provide.
Labels (1)
0 Kudos
0 Replies