Content originally posted in LPCWare by Aditya Mittal on Sun Apr 05 23:18:41 MST 2015
Hello,
To start off with I am planning to move ahead with USB CDC class for Virtual com. I have taken reference from the sample codes available.
I can now run my program, and when I plug in my device to Windows (XP and Win7) machine, it detects as VCOM device, however it asks for the installation of drivers. I know a little bit that I am required either to generate/modify/install the INF file for this device to work properly, but I am not able to understand how to do that. I have taken the sample INF file already available with example codes (attached for reference, changed the extension of the file from INF to TXT), but I don't know exactly how to use it.
Do I require some kind of patch to install this file or do I need to keep this file in WINDOWS folder at some particular location?
I also tried to manually navigate and browse to the path where I kept this file when windows asks to manually install the driver, but still the same results.
Can any one help me out with this problem?
Thanks in advance.
Aditya