Content originally posted in LPCWare by j.daheron on Fri Jul 27 01:11:00 MST 2012
Hi,
I'm developing a Mass Storage Device application using nxpUSBlib v0.95 running on LPC1850 (Keil MCB1800 Dev. Board).
I work on example code provided with the library, but I've changed the virtual disk to be in RAM area (some kB only).
The application works fine when running from RAM (like in the example), but the device is not recognized when the application runs from SPIFI.
Could someone help me to understand why ?
Thanks,
--
Julien