lpcware

Voltage regulator and current sense for LiPo batteries

Discussion created by lpcware Employee on Jun 15, 2016
Latest reply on Jun 15, 2016 by lpcware
Content originally posted in LPCWare by jhd on Tue Dec 01 17:50:25 MST 2015
Hello,

Sorry if this post is not here, I did not know where to put it.

I need to build a voltage regulator and monitor current and voltage sense for LiPo batteries. 2S to 8S or 10S if is possible.

With this features:

V Input: from 7,4V up-to 50-60V
Current max.: 175A

V Out: 5V
Current Out: about 3A

And a 5V to 3,3V converter to supply providing of LPC54102, Bosch sensors, and other components in the pcb (all works to 3,3V), but other external periphericals works to 5V.


Best regards.

Outcomes