MPC5675K FEC bug in DPM mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5675K FEC bug in DPM mode

1,040 Views
danielsommer
Contributor I

Hello all,

 

I have an Ethernet testing code running on MPC5675K, which is working correctly using Lockstep mode. As soon as I switched to DPM, I am experiencing an interesting problem. When a message is received, the Rx interrupt is initiated and I check the content of the according receive buffer. The start of the package (8 bytes) is correct, but after that the rest of the package is mixed up in the memory.

Correct version (LSM - buffer starts at 0x40003368):

153592_153592.pngLSM_marked.png

Buggy version (DPM - buffer start at 0x40003378):

153665_153665.pngDPM_marked.png

 

Do you have any idea of the root cause?

 

Thank you in advance for your help!

Daniel

Labels (1)
0 Kudos
4 Replies

731 Views
danielsommer
Contributor I

Thank you, I will investigate this.

0 Kudos

731 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

the first thought could be disabling the cache at all, or with the help of MMU disable caching of the memory areas where TX/RX Buffer descriptors and TX/RX buffers are placed.

BR, Petr

0 Kudos

731 Views
danielsommer
Contributor I

Hi,

thank you for you help!

Could you give me some directions, how I can disable the cache? Or configure MMU? I didn't find any related information in the reference manual...

Thank you again!

0 Kudos

731 Views
PetrS
NXP TechSupport
NXP TechSupport

The easiest way could be disabling the cache at startup, if enabled there. Not sure what IDE you are using, so go through startup code and comment out related code.

The device Core manual describes both the Cache and MMU modules; http://cache.nxp.com/files/32bit/doc/ref_manual/e200z760RM.pdf

You can also look at following document and read chapters MMU and Cache; e200 Core Training relevant to MPC55xx and MPC56xx device family.

For the MMU setup the MMU Assist Register CONFIGURATOR can be used.

0 Kudos