AnsweredAssumed Answered

PTB0/1 and PTB10/11 are swapped on FRDM-KL82Z pinout

Question asked by Matthias Jugel on Jun 15, 2016
Latest reply on Jun 16, 2016 by Matthias Jugel

Is it possible that the pinout of the Quick Start Guide for the FRDM-KL82Z board has the pins PTB0/1 and PTB10/11 mixed up?

 

I looked at the KL82 sub family documentation and tried to use I2C0 on PTB0/1. When I didn't get a signal, I checked the pins PTB10/11 and there was the signal. Vice versa, using I2C1 I got the signal on PTB0/1 instead. On the board these are Pins 10/12 and 18/20 respectively.

 

It is not a problem as such, but confusing.

 

Thanks,

 

Leo.

Outcomes