Why intrenal regulator o/p (VDDA) of MC13213 is 2.23V isntead of 1.8V?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why intrenal regulator o/p (VDDA) of MC13213 is 2.23V isntead of 1.8V?

1,480 Views
lekkal
Contributor I
Hi all,

 I am getting output of internal regulator of MC1321x is 2.23V i.e., pin No 32, VDDA. It is suppose to be 1.8V. When I removed the external crystal oscilltor(16MHz) the internal regulator output is 1.8V. I am unable to get the same 1.8V output with external crystal oscillator is introducing on the board. 3 modules are assembled and found the same problem in all of them.

The board contains:
1. MC13213
2.16MHz Crystal Oscillator


1. No extrenal baluns
2. No external switch

Why I am getting VDDA 2.23V istead of 1.8V, how the crystal effects regulator output?

Thanks inadvance.
Labels (1)
0 Kudos
2 Replies

293 Views
Denn
Contributor I
Hello,
 
 
Also refer the AN on Improving the Transient Immunity Performance of Microcontroller-Based Applications
 
 
 
 
 
Regards,
Denn
0 Kudos

293 Views
bigmac
Specialist III
Hello,
 
It would seem that VddA is pin 33, rather than pin32.  So possibly you might be measuring the wrong pin.  Pin 32 is Vbat.
 
Have you used all the supply bypass capacitors as specified in the datasheet, and do you have proper grounding to a ground plane layer? The only explanation I can think of is that you are "picking up" some of the RF signal from the crystal, and this is imposing itself on your voltage measurement.  This would be more likely to occur with poor bypassing or grounding.
 
Regards,
Mac
 
0 Kudos