can gpio of imx6q set output to tri-stated?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can gpio of imx6q set output to tri-stated?

524 Views
翔李
Contributor IV

hi,

Can the gpio of imx6q,output to tri-stated?if it can,how to set up it to tri-stated output? I now want to set gpio1_27 to output and tri-stated at sometimes.

thanks.

Tags (1)
0 Kudos
1 Reply

366 Views
art
NXP Employee
NXP Employee

There is no special 'tri-stated output' setting for the i.MX6 GPIO signals. To make a GPIO signal act as tri-state, you have to switch it to Input mode.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos