Hello Wagan,
I am not sure how to check the version because I don't have physical access to the board.
Here is what I have, Let me know if there is anything to check. The issue is that after booting over the cs8900_eth0, I can configure the FEC using ifconfig and access the system on that interface.
Thanks,
zbsar
++... Read from 0x07ee0000-0x07f00000 at 0xc1fe0000: .
... Read from 0x07ed3000-0x07ed4000 at 0xc1fff000: .
Ethernet FEC MAC address: 00:04:9f:00:63:55
Board Type: ADS
Clock input: 26 MHz
Booting from [NOR flash]
FEC: [ HALF_DUPLEX ] [ disconnected ] [ 10M bps ]:
Ethernet eth0: MAC address 00:00:00:00:00:00
IP: 128.224.165.54/255.255.255.0, Gateway: 128.224.165.1
Default server: 128.224.165.20
RedBoot(tm) bootstrap and debug environment [ROMRAM]
Non-certified release, version FSL 200712 - built 14:16:56, Mar 20 2007
Platform: MX27 ADS/EVB (Freescale i.MX27 based) PASS 1.0 [x32 SDR]
Copyright (C) 2000, 2001, 2002, 2003, 2004 Red Hat, Inc.
RAM: 0x00000000-0x07f00000, [0x00025140-0x07ed1000] available
FLASH: 0xc0000000 - 0xc2000000, 256 blocks of 0x00020000 bytes each.
== Executing boot script in 2.000 seconds - enter ^C to abort