JimDon, no I am now using my target board. To program and test my targets (which have very small pitch connectors), I use a programming fixture board which has the BDM connector, power input, test buttons, etc.
I've attached a schematic page of this fixture board to show how it's set up.
The upper left corner is a 3.3V regulator. I have found that my Rev B Cyclone requires the VCC pin in order to work properly. Hence, in the lower left corner, the switch must be turned to the Cyclone Program option.
The upper right corner is power in to the fixture which powers my target as well. The lower left corner is a reset circuit which I devised to help condition the BKGD pin when using a USB Multilink and attempting to program blank MC9S08QGx parts. It's a known situation, talked about at length here on the forums. The switch in my ciruit is a failsafe, allowing me to manually hold BKGD low during power up just in case. For what it's worth, I have found that I need this reset BKGD circuit only 5% of the time. For production programming, I have jumper JP1 set to inactive state.
As I said before, my target has pullups on the RST and BKGD pins.