1. I use the following command to do USB OTG Eye Diagram test:
./memtool -32 0x020c9010=0x10000007
./memtool -32 0x02184140=0x2
./memtool -32 0x021841A8=0x3
./memtool -32 0x02184184=0x1C0400001
2. USB OTG Eye Diagram test failed on Yocto 3.14.52_1.1.0_ga.
But USB OTG Eye Diagram test passed on Yocto 3.14.38_beta.
Attached file includes USB OTG Eye Diagram test pictures.
Can you help solve this issue?
Thank you.
Best Regards,
Alex
Original Attachment has been moved to: USB-OTG-Eye-Diagram-test-picture.zip
Hi charles
one can check and compare usb phy settings described in
sect.4.3.3 Operational settings AN4589 Configuring USB on i.MX 6 Series
Processors
http://cache.nxp.com/files/32bit/doc/app_note/AN4589.pdf
In general "beta" linux release can not be considered as reliable.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------