puneeth NS

Channel interrupts not working in Full Chip simulation

Discussion created by puneeth NS on Mar 29, 2008
Latest reply on Apr 4, 2008 by bigmac
Hello,

       Using MC9S08AW16 processor, when I use debugger in Full Chip mode, the channel interrupts dont occur at al. But when I burn the program on the chip it works fine. Using codewarrior v5.7. I have set the frequency as ~19 MHz, but the P&E Multilink debugger reduces the frequecy to ~17MHz, it changes even if i put other frequencies.

Outcomes