Hi.
I am working with KS8999 as switch. I want to connect it with a Ethernet phy from backplane, The KS8999 Analog Voltage is 2Volt and Ethernet PHY voltage is 2.5Volt. I am confused.
Any body can help me about these connections? can I connect these interface to each other?
Have a great day,
The ks8999 data sheet
http://ww1.microchip.com/downloads/en/DeviceDoc/ks8999%20Data%20Sheet.pdf
says " Single 2.0V power supply with options for 2.5V and 3.3V I/O" and we can see special pins for I/O power in the Pin Description table "VDD-IO Pwr 2.0V, 2.5V or 3.3V for I/O circuitry". So ks8999 I/O can be connected to the device with 2.5V interface.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Serguei,
I know that KS8999 can work with 2.5Volt. But I design a daughter board that connect with the main board. In main board I have ks8999 and I cant change it.
If I connect a 2.5Volt ethernet PHY to a 2Volt ethernet PHY, does it working? How connect them without magnetic?