Hi,
I want to use both CAN ports on my iMX6 Quad Plus + Sabre Automotive Base Board (+ Atheros GBit Ethernet).
The problem is that only a single one (CAN2) is available in Linux (as "can0").
I'm using bitbake from the Yocto project to build the SD-card image with Linux.
BSP: FSL Community BSP
Build Configuration file "local.conf" (excerpt):
MACHINE ??= 'imx6qpsabreauto'
DISTRO_FEATURES_remove = "x11 wayland directfb "
IMAGE_INSTALL_append = "iproute2 libsocketcan canutils"
Build command:
bitbake core-image-minimal
According to some other answers in this community portal I've added "can0" to the kernel boot arguments, but it does not help.
The boot log contains only a message that a single can device was registered.
root@imx6qpsabreauto:~# dmesg | grep can
Kernel command line: console=ttymxc3,115200 root=/dev/mmcblk2p2 rootwait rw can0
2094000.can supply xceiver not found, using dummy regulator
flexcan 2094000.can: device registered (reg_base=f0238000, irq=143)
can: controller area network core (rev 20120528 abi 9)
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20120528 t)
can: netlink gateway (rev 20130117) max_hops=1
CAN2 is available as "can0" in Linux and works after configuration:
root@imx6qpsabreauto:~# ifconfig -a
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:143
eth0 Link encap:Ethernet HWaddr 00:04:9F:03:D9:86
inet6 addr: fe80::204:9fff:fe03:d986/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:106 errors:0 dropped:0 overruns:0 frame:0
TX packets:30 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:12550 (12.2 KiB) TX bytes:8172 (7.9 KiB)
root@imx6qpsabreauto:~# ip link set can0 up type can bitrate 500000
flexcan 2094000.can can0: writing ctrl=0x03292005
How can I enable CAN1 ?
Thank You.
Solved! Go to Solution.
Hi Stefan
it is necessary to use zImage-imx6qp-sabreauto-flexcan1.dtb
configuration, as flexcan1 is disabled by default in standard DTB file due to
pin conflicts with FEC. Please refer to attached Release Notes Table 3. Kernel
and device tree configurations.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Stefan
it is necessary to use zImage-imx6qp-sabreauto-flexcan1.dtb
configuration, as flexcan1 is disabled by default in standard DTB file due to
pin conflicts with FEC. Please refer to attached Release Notes Table 3. Kernel
and device tree configurations.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------