USB 4.1.1 USBERR_DEVICE_BUSY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB 4.1.1 USBERR_DEVICE_BUSY

350 Views
Mike_d
Contributor IV

Hi,

I often end up with a USBERR_DEVICE_BUSY error from using the USB_Class_CDC_Interface_DIC_Send_Data() function.

How do I recover my interface at this point?

Thanks,

-Mike

0 Kudos
1 Reply

232 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mike,

Thanks for your interest in NXP Semiconductor products and the opportunity to serve you.

I was wondering if you can illustrate the detail procedure to replicate the issue, then it will help me to investigate the issue.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos