Hi,
We have a network (floating) license for Codewarrior Classic 5.2. After a few build's of my software, the linker error "L4025: This limited version allows only 65536 bytes of C code" appears and the link failed. When i wait a minute or two, and build again, it works as exprected.
We also use Codewarrior 10.6 with the same license model - without problems.
Thank you in advance!
Adrian
Solved! Go to Solution.
It will be good to see the log file located in LMTools.exe utility , also wondering if you are using comm
Check the log file on the path specified
If you are using multiple clients, sometime check in does not occur right away this might be a root cause.
It will be good to see the log file located in LMTools.exe utility , also wondering if you are using comm
Check the log file on the path specified
If you are using multiple clients, sometime check in does not occur right away this might be a root cause.