i.MX6Q Sabre Android Emulator on WinCE7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q Sabre Android Emulator on WinCE7

414 Views
wayne7215
Contributor I

Hi

We use the i.MX6Q Sabre for our application running on WinCE7 (or Windows embedded 7 compact) and we would like to run an Android Emulator on it. Is that anyhow possible? I've just read that the MX6Q is fully supported for Android, but how does it look when we still would keep WinCE7 as OS but run an Emulator for Android on it?

I would really appreciate any feedback or instructions how we could do it :-)

Thank you

Tags (2)
0 Kudos
1 Reply

263 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Marco,

There are also available BSPs for Android on i.MX6Q devices (including 4.x, 5.x and 6.x releases) as native operating system; however, emulators are not provided by NXP.

Regarding Windows BSPs support for i.MX, Deactivated user could provide additional details.

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos