AnsweredAssumed Answered

Changing The Boot console

Question asked by hrushinale on Jun 10, 2016
Latest reply on Jun 10, 2016 by igorpadykov

HI ,

                          I am  facing the problem related to serial console . The default console given for our board is at UART1 bu I change it to UART 2.For that I made the below changes in U-boot:

#define CONFIG_MXC_UART_BASE    UART2_BASE

#define CONFIG_CONSOLE_DEV        "ttymxc1"

 

also configured the UART in customboard.c file like

iomux_v3_cfg_t const uart2_pads[] = {

    MX6_PAD_SD3_DAT5__UART2_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),

    MX6_PAD_SD3_DAT4__UART2_RX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),

    MX6_PAD_SD3_CMD__UART2_RTS_B | MUX_PAD_CTRL(UART_PAD_CTRL),

    MX6_PAD_SD3_CLK__UART2_CTS_B | MUX_PAD_CTRL(UART_PAD_CTRL),

};

 

 

static void setup_iomux_uart(void)

{

    imx_iomux_v3_setup_multiple_pads(uart1_pads, ARRAY_SIZE(uart1_pads));

    imx_iomux_v3_setup_multiple_pads(uart2_pads, ARRAY_SIZE(uart2_pads));

}

int board_early_init_f(void)

{

    setup_iomux_uart();

}

 

After doing all these changes when we connect the board its showing garbage value.. But when kernel is loaded then its showing messages on UART2.Please Suggest the solution.

 

 

Regards,

hrushi

Outcomes