Android Emulator on WinCE7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Emulator on WinCE7

556 Views
wayne7215
Contributor I

Hi

We use the i.MX6Q Sabre for our Application based on a WinCE7 OS. Now we would like to know if it's possible to run a Android Emulator on the WinCE7 OS instead of replacing the entire WinCE7 with Android.

Any expiriences with an Emulator and would it support also all the Interfaces of the undelaying WinCE7 OS?

We would really appreciate any recommendation or instructions how to do it if it's possible.

Thx

Labels (3)
0 Kudos
1 Reply

385 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Marco,

There are also available BSPs for Android on i.MX6Q devices (including 4.x, 5.x and 6.x releases) as native operating system; however, emulators are not provided by NXP.

Regarding Windows BSPs support for i.MX, Adeneo Engineering Team could provide additional details.

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos