AnsweredAssumed Answered

Can we use a pin other than Port A18 to pick up the 50MHz clock in..?

Question asked by Ken Armitage on Jun 8, 2016
Latest reply on Jun 10, 2016 by Jorge Antonio Alcala Vazquez

We have a custom K60DN512-based board which uses a 50MHz external clock input to the processor on PTA18 just like the TWR-K60D100M board. Unfortunately one of the printed circuit boards has lost the pad at M12, so we can't use the PTA18 input. Is it possible to re-programme the device to look for the clock on a different I/O pin or port...?

 

We are using Codewarrior V10.6 and running MQX4.1.

 

Thanks

 

Ken

Outcomes