Question, i.MX6SX unused pin handling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6SX unused pin handling

Jump to solution
511 Views
Aemj
Contributor IV

Dear team,

I would like to ask about the recommended connections for unused analog interfaces of i.MX6SoloX.

In i.MX6SX datasheet(IMX6SXCEC Rev.1), it is described in Table-5 that the recommended connection of unused VADC_IN[0:3] is float.

But in i.MX6SX hardware design guide(IMX6SXHDG, Rev.1), the recommended connection for unused VADC_IN[0:3] is said as connect to GND, in table-2-17.

Which is the truth?

I found difference on the recommended connections for unused VDD_AFE_1P2 and VDDA_AFE_3P3 as well between datasheet and hardware design guide.

Please show me which is correct about VDD_AFE_1P2 and VDDA_AFE_3P3 as well.

Thanks,

Miyamoto

Labels (1)
0 Kudos
1 Solution
425 Views
Yuri
NXP Employee
NXP Employee

Hello,


  from the design team :

1. VADC_IN[3-0] can be grounded or float when they are not used.

2. VDD_AFE_1P2 and VDD_AFE_3P3 should be grounded when they are not used.

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
426 Views
Yuri
NXP Employee
NXP Employee

Hello,


  from the design team :

1. VADC_IN[3-0] can be grounded or float when they are not used.

2. VDD_AFE_1P2 and VDD_AFE_3P3 should be grounded when they are not used.

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

------------------------------------------------------------------------------

0 Kudos