AnsweredAssumed Answered

Are the differential pressure sensors suited to be used with diesel or petro fuel mediums ?

Question asked by Zeeshan Noorwala on Jun 5, 2016
Latest reply on Jun 8, 2016 by David Diaz Marin

I am trying to develop a Fuel level monitoring data aquisition system, and therefore i am selecting MPX2053 and similar sensors for upto 4 meters of fuel height in tank.

 

What i want to know is, are these differential pressure sensors suited to be used with Diesel and/or Petro fuels ?

 

If not, can you suggest which alternate sensors or methods i may use for my application ?

 

One option was to use a Stainless steel based Differential pressure Transmitter (4 to 20 mA output) and connect it to my system. This, is a ready built solution but is very costly compared to discrete sensors based system. Therefore i am prefering to use sensors from NXP / Freescale, as i have had previous experiecne with the same in a different application.

 

Thank you.

 

Regards,

Zeeshan

Outcomes