pfuze100-regulator 1-0008: unrecognized pfuze chip ID!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pfuze100-regulator 1-0008: unrecognized pfuze chip ID!

2,785 Views
fulinux
Contributor IV

Dear community:

Hardware Platform:

Processor: Freescale i.MX6Q

Memory: DDR3 4GB

Flash: 32GB Managed Nand

 

Software Platform:

Kernel: linux 4.1.15

BSP: imx_4.1.15_1.0.0_ga

 

i add this in my dts file for pfuze100:

&i2c2 {

  clock-frequency = <100000>;

  pinctrl-names = "default";

  pinctrl-0 = <&pinctrl_i2c2>;

  status = "okay";

 

 

  pmic: pfuze100@08 {

  compatible = "fsl,pfuze100";

  reg = <0x08>;

  pinctrl-names = "default";

  pinctrl-0 = <&pinctrl_pfuze>;

  interrupt-parent = <&gpio7>;

  interrupts = <13 2>;

 

 

  regulators {

  sw1a_reg: sw1ab {

  regulator-min-microvolt = <300000>;

  regulator-max-microvolt = <1875000>;

  regulator-boot-on;

  regulator-always-on;

  regulator-ramp-delay = <6250>;

  };

 

 

  sw1c_reg: sw1c {

  regulator-min-microvolt = <300000>;

  regulator-max-microvolt = <1875000>;

  regulator-boot-on;

  regulator-always-on;

  regulator-ramp-delay = <6250>;

  };

 

 

  sw2_reg: sw2 {

  regulator-min-microvolt = <800000>;

  regulator-max-microvolt = <3300000>;

  regulator-boot-on;

  regulator-always-on;

  regulator-ramp-delay = <6250>;

  };

 

 

  sw3a_reg: sw3a {

  regulator-min-microvolt = <400000>;

  regulator-max-microvolt = <1975000>;

  regulator-boot-on;

  regulator-always-on;

  };

 

 

  sw3b_reg: sw3b {

  regulator-min-microvolt = <400000>;

  regulator-max-microvolt = <1975000>;

  regulator-boot-on;

  regulator-always-on;

  };

 

 

  sw4_reg: sw4 {

  regulator-min-microvolt = <800000>;

  regulator-max-microvolt = <3300000>;

  };

 

 

  swbst_reg: swbst {

  regulator-min-microvolt = <5000000>;

  regulator-max-microvolt = <5150000>;

  regulator-boot-on;

  regulator-always-on;

  };

 

 

  snvs_reg: vsnvs {

  regulator-min-microvolt = <1000000>;

  regulator-max-microvolt = <3000000>;

  regulator-boot-on;

  regulator-always-on;

  };

 

 

  vref_reg: vrefddr {

  regulator-boot-on;

  regulator-always-on;

  };

 

 

  vgen1_reg: vgen1 {

  regulator-min-microvolt = <800000>;

  regulator-max-microvolt = <1550000>;

  };

 

 

  vgen2_reg: vgen2 {

  regulator-min-microvolt = <800000>;

  regulator-max-microvolt = <1550000>;

  };

 

 

  vgen3_reg: vgen3 {

  regulator-min-microvolt = <1800000>;

  regulator-max-microvolt = <3300000>;

  };

 

 

  vgen4_reg: vgen4 {

  regulator-min-microvolt = <1800000>;

  regulator-max-microvolt = <3300000>;

  regulator-always-on;

  };

 

 

  vgen5_reg: vgen5 {

  regulator-min-microvolt = <1800000>;

  regulator-max-microvolt = <3300000>;

  regulator-always-on;

  };

 

 

  vgen6_reg: vgen6 {

  regulator-min-microvolt = <1800000>;

  regulator-max-microvolt = <3300000>;

  regulator-always-on;

  };

  };

  };

};

 

it shows some wrong in kernel log as follows:

pfuze100-regulator 1-0008: unrecognized pfuze chip ID!

pfuze100-regulator: probe of 1-0008 failed with error -5

 

what is wrong? @log file attached here

Original Attachment has been moved to: imx6q-klsw.dts.zip

Original Attachment has been moved to: dmesg.log.zip

Labels (3)
Tags (1)
0 Kudos
4 Replies

1,540 Views
marcocavallini
Contributor V

I had the same problem,

everything was fine using kernel 3.10.17 but then migrating to 4.1-2.0 it failed.

pfuze100-regulator 1-0008: unrecognized pfuze chip ID!
pfuze100-regulator: probe of 1-0008 failed with error -5

The solution was to set up the proper pinctrl-0 value

&i2c2 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c2_1>;
status = "okay";

Because setting the wrong set of MUXes would result in a I2C read/write bus failure.

This is the final result:

pfuze100-regulator 1-0008: Full layer: 2, Metal layer: 1
pfuze100-regulator 1-0008: FAB: 0, FIN: 0
pfuze100-regulator 1-0008: pfuze100 found.

Distinti Saluti / Best Regards
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded software engineering
http://KoanSoftware.com

0 Kudos

1,540 Views
yakovshaulov
Contributor II

Hello Chen,

Have you solved this issue?

We have the same problem, except that our PMIC is PF3000 and we saw the same message appears at Kernel log:

pfuze100-regulator 0-0008: unrecognized pfuze chip ID!
pfuze100-regulator: probe of 0-0008 failed with error -110

Thanks.

0 Kudos

1,540 Views
igorpadykov
NXP Employee
NXP Employee

Hi

that message is printed from pfuze_identify() in

linux-2.6-imx.git - Freescale i.MX Linux Tree

so one can add additional  debug  printfs to identify problem.

What is MMPF0100 marking, is it detected correctly in uboot ?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,540 Views
fulinux
Contributor IV

Hi igor,

     thank you for your feedback, our hardware has no problem, because kernel in imx_3.0.35_4.1.0 version can register and operate pfuze100, look at this:

P60603-183750.jpg

do you need any information? pls tell me.

thank you,

fulinux.

0 Kudos