iMX6Q : How to work a software reset ( set SRC_SCR register ) ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q : How to work a software reset ( set SRC_SCR register ) ?

Jump to solution
603 Views
koichisakagami
Contributor II

Dear community,
I am checking a SRC_SCR register coreX_rst field. (X is 0,1,2,3)

In the case of setting a coreX_rst field , does the reset process begin immediately ?

Or , after performing any process , does the reset process subsequently begin ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
1 Solution
393 Views
Yuri
NXP Employee
NXP Employee

Hello,

  timings for the secondary CPU reset are not specified, since this

is mainly software, not hardware, process.

"Once the bits are set, the corresponding core is released from its reset state,

and it executes the boot ROM (at 0000 0000h). The boot ROM determines if it
is a secondary core and uses the persistent bit registers to determine what to
execute next."

Have a great day,
Yuri
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
394 Views
Yuri
NXP Employee
NXP Employee

Hello,

  timings for the secondary CPU reset are not specified, since this

is mainly software, not hardware, process.

"Once the bits are set, the corresponding core is released from its reset state,

and it executes the boot ROM (at 0000 0000h). The boot ROM determines if it
is a secondary core and uses the persistent bit registers to determine what to
execute next."

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos