AnsweredAssumed Answered

About  initialization time of ERR007926 in i.MX6DQ.

Question asked by Keita Nagashima on Jun 1, 2016
Latest reply on Aug 10, 2017 by Perry GUTTIN-LOMBARD

Hi All,

 

Refer to ERR007926 in IMX6DQCE(Rev.6).

There is below description in SDMMC boot Workaround.

"SD/MMC: Choose an SD/MMC card for which the Nac parameter is to be specified less than

50 ms and its initialization time is less than 500 ms."

 

I think that Nac parameter is TAAC + NSAC from SD Specification.

But, I didn't find the parameter of "initialization time".

Could you tell me the parameter?

 

Best Regards,

Keita

Outcomes