Reading DIMM SPD using CW 10.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading DIMM SPD using CW 10.5

724 Views
sureshk
Contributor II

Hi,

      I am planning to generate DDR configurations by reading DIMM SPD in Codewarrior eclipse 10.5 version. I am using CWTAP USB version. Kindly help me with  the probe type ID i have to provide in the below screenshot.

 

 

152710_152710.pngpastedImage_0.png

 

      and clarify , how JATG will read SPD ? does it require to load basic .tcl before reading SPD?

 

Regards,

  suresh

Labels (1)
0 Kudos
2 Replies

562 Views
addiyi
NXP Employee
NXP Employee

If you are using CWTAP over usb, and this is the only tap probe connected to your machine, is not required to enter any TAP ID. Just select Probe: CWTAP and click on Read SPD.

SPD data is read from the DIMM using an application which is running when Read SPD button is press. This process is transparent for users.

Adrian

0 Kudos

562 Views
sureshk
Contributor II

Thank you Adrina. It is reading SPD even if i leave probe ID blank.

Regards,

  suresh kalepu

0 Kudos