What is the silicon revision of the LS1021A mounted at the TWR-LS1021A 700-28040 REV C board?
I am asking this because I want to know whether I should use QorIQ SDK V1.8 (which supports rev 1.0) or QorIQ SDK V2.0 (which support revision 2.0).
Solved! Go to Solution.
The silicon revision should be 1.0.
To doublecheck please power-on the board and inspect the U-Boot console output.
De U-Boot console output shows revision 1.0:
U-Boot 2014.01Layerscape-SDK-V1.3+g50d6848 (Oct 24 2014 - 19:21:22)
CPU: Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)
Do all TWR-LS1021A board have a silicon revision 1.0? If not which TWR-LS1021A revision(s) have a 2.0 silicon?
I am asking this because we want to use the silicon 2.0 for our product I want to evaluate the latest Linux QorIQ SDK.
TWR-LS1021A-PB has silicon revision 2.0
The silicon revision should be 1.0.
To doublecheck please power-on the board and inspect the U-Boot console output.