AnsweredAssumed Answered

is it possible to turn RF field on without pn532 going into power down mode?

Question asked by Eveline Ververgaert on May 30, 2016
Latest reply on Jun 14, 2016 by Jorge_Gonzalez

Dear fellow programmers,

 

For my team test suite (a project for school) it is required to turn the RF field on (on the Adafruit pn532 break out board).

I found a way to turn it on, but it refuses to stay on: (partial of the code comes from the adafruit pn532 library)

 

bool AdafruitPn532Extended::SetFieldOn()

{

  commandbuffer[0] = PN532_COMMAND_RFCONFIGURATION;

  commandbuffer[1] = 0x01;

  commandbuffer[2] = 0x01;

 

  if (!sendCommandCheckAck(commandbuffer, 3))

  {

     return 0x0;  // no ACK

  }

  return 1;

}

 

I also tried:

 

bool AdafruitPn532Extended::CheckForReadableTarget()

{

  uint16_t timeout = 0;

  //setPassiveActivationRetries(0xFF);

 

  commandbuffer[0] = PN532_COMMAND_INLISTPASSIVETARGET;

  commandbuffer[1] = 1;  // max 1 cards at once (we can set this to 2 later)

  commandbuffer[2] = PN532_MIFARE_ISO14443A;

 

  if (!sendCommandCheckAck(commandbuffer, 3, timeout))

  {

    return 0x0;  // no cards read

  }

  return 1;

}

 

With this code it works once, then I have to manual remove the tag or adafruit-PN532 breakout shield in order for it to work again.

 

My best guess is, it's either the first one where power down mode has to be turned off in a way. Or the second option where most probably I have to trick the RF field detection into thinking a new tag was placed in the field.

 

I thank you very much for your time.

Outcomes