I'm generatin a new RCW with QCVS 4.5 for a T2080 board.
When I try to configure RCW_SRC, PBI_SRC and BOOT_LOC to NOR Flash, QCVS shows an error, why?
When I change PBI_SRC or BOOT_LOC to another interface there is no error.
If I try the same configuration with previous versions of QVCS (4.2.1) there is no error for this configuration.
Please upgrade to QCVS 4.5 which is the latest release.
Adrian
Ok, after update no error is show.
Thank you.
De: addiyi
Enviado el: lunes, 30 de mayo de 2016 13:23
Para: Hernández Sánchez, Sergio
Asunto: Re: - QCVS error configuring NOR FLASH
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
QCVS error configuring NOR FLASH
reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655533?et=watches.email.thread#comment-655533>
It is just an warning. You can ignore it by selecting Advanced tab and Ignore Constrains and Non-Critical errors.
Adrian
Ok, but why it is considered an ERROR, I think it is a valid configuration.
De: addiyi
Enviado el: lunes, 30 de mayo de 2016 9:38
Para: Hernández Sánchez, Sergio
Asunto: Re: - QCVS error configuring NOR FLASH
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
QCVS error configuring NOR FLASH
reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655446?et=watches.email.thread#comment-655446>
Could you add your PBL binary? Also, what Soc rev have you selected?
Adrian
I’ve selected V1.1
PBL generated is attached to this email.
De: addiyi
Enviado el: lunes, 30 de mayo de 2016 10:15
Para: Hernández Sánchez, Sergio
Asunto: Re: - QCVS error configuring NOR FLASH
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
QCVS error configuring NOR FLASH
reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655496?et=watches.email.thread#comment-655496>
No error on my side:
Could you please provide the QCVS build number. Go to Help > About CodeWarrior, click on QCVS icon and provide the version number.
Adrian
I’m using eclipse version installed in VirtualBox provided by NXP witk SDK 1.9
De: addiyi
Enviado el: lunes, 30 de mayo de 2016 12:56
Para: Hernández Sánchez, Sergio
Asunto: Re: - QCVS error configuring NOR FLASH
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
QCVS error configuring NOR FLASH
reply from Adrian-Mihai Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in QorIQ Processing Platforms - View the full discussion<https://community.nxp.com/message/655531?et=watches.email.thread#comment-655531>