Hi,
We have requirement for data path routing in LS1021A-IOT board. Does it supports
In SDK documentation these feature are not applicable for IOT board. Could someone tell how to enable them on LS1021A-iot?
Regards,
Anil
LS1021A is not equipped with DPAA, therefore, none of DPAA components,
such as QMAN, FMAN, BMAN or RMAN is available in this processor.
LS1021A Ethernet controllers, eTSECs, however, are equipped with a frame
parser/filer (see LS1021ARM, Section 20.9.4) which allows ASF to be
supported on your device. Refer to your board SDK documentation for
more details:
Have a great day
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------