AnsweredAssumed Answered

Question about PTN3356

Question asked by Luca Rigazio on May 27, 2016


Hello,

 

I need to design a DisplayPort to VGA converter that works from -20° C to 85° C. PTN3356 would be perfect, but it does not work below 0° C. Are there any other solutions with NXP products? Which issues could I run into if I insist working with that device below 0° C ? Is there any way of getting samples tested/qualified in the industrial temperature range?

 

Thanks

Outcomes