Using one of the driver examples for FRDM-KL03 (e.g. adc16). KSDK1.3 and KDS 3.0.
What needs to be changed to target 8K Flash version of the KL03 instead of the 32K version? Is it just the linker file?
Solved! Go to Solution.
Hi,
Because the chip is the same, just flash or RAM size are different, so i think it is okay for you just to update the linker file, chnange memory address and length in linker file.
Hope it can help you.
BR
Xiangjun Rong
Hi,
Because the chip is the same, just flash or RAM size are different, so i think it is okay for you just to update the linker file, chnange memory address and length in linker file.
Hope it can help you.
BR
Xiangjun Rong