SDRAM CLK Assignment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDRAM CLK Assignment

Jump to solution
537 Views
mrudangshelat
Contributor IV

Hi, I was referring SABRESDB (SPF-27516_C5) for my ongoing design. Is there any specific reason to assign SDCLK1 to Lower DATABUS DRAM_D[31:0] and SDCLK0 to Higher DATABUS DRAM_D[63:32]? I would like to know because generally I have seen SDCLK1 to higher DATABUS DRAM_D[63:32 and SDCLK0 to lower DATABUS DRAM_D[31:0]. Regards, Mrudang

Labels (2)
1 Solution
423 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

there is no special reason as both signals are identical.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
424 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

there is no special reason as both signals are identical.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

423 Views
mrudangshelat
Contributor IV

Hi Igor,

If I use CLK1 instead of CLK 0 for lower data-bus D[15:0], A[15:0] and other controller will be having interfaced on CS0, CKE0 and ODT0.

  1. Does it effect power consumption of DDR SDRAM?
  2. Do iMX6 has Single or Dual DDR Controller/channel?

Regards,

Mrudang

0 Kudos