AnsweredAssumed Answered

Problem with Pegoda reader and Mifare Desfire V1 card

Question asked by Hermann Zheboldov on May 23, 2016

Hello,

I'm writing test program for Mifare Desfire V1 card and find the following problem. When I send "Select Application" command to the card via Omnikey 5321 v2 CL SAM reader I have got the following log:

 

Mon May 23 09:42:30 2016

REQUEST:

Command =  0x5A 0x00 0x00 0x00

Request Lenght = 4

Request protocol = CL

 

 

  >> 5A 00 00 00

 

 

RESPONSE:

  <<Response Lenght = 1

Response status = 0x00000000 - SCARD_S_SUCCESS

 

 

  << 00

-------------------------------------------------------------------------

This is a normal answer, all is Ok.

When I send the same command to the RD710 reader I have got the following:

 

Mon May 23 10:00:12 2016

REQUEST:

Command =  0x5A 0x00 0x00 0x00

Request Lenght = 4

Request protocol = CL

 

 

  >> 5A 00 00 00

 

 

RESPONSE:

  <<Response Lenght = 6

Response status = 0x00000000 - SCARD_S_SUCCESS

 

 

  << 5A 80 25 01 00 00

-------------------------------------------------------------------------

 

Can anybody explain me for what reason I receive such an answer from the card?

Outcomes