AnsweredAssumed Answered

SDK 1.3 - KV10Z128 issue with IAR7.60.1

Question asked by q1444 Employee on May 19, 2016
Latest reply on May 19, 2016 by Iva Susnova

Hi all,

customer discovered an issue with the "Hello World" example for the KV10Z128 in SDK1.3.

When working with the standard settings of the project for KV10Z128 then the flashloader "KVxx128K.flash" is used and causes an abort of the flash process.

However when uisng the KV11 flashloader "KV11128K.flash" for the KV10Z128 project then everything works fine.

File compare shows difference in the <block> section for both devices although they should have identical settings.

(See file comparison:)



   
Please follow up with SDK1.3 responsible people and IAR if necessary to get that corrected.
 

br

Guenter

Outcomes