Eval install of CW 10.6.4 runs into error when importing CW 7.3 project for 56F8345

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eval install of CW 10.6.4 runs into error when importing CW 7.3 project for 56F8345

298 Views
michaelmojadad
Contributor I

Hi,

 

I have installed CV 10.6.4 and tried to import (file->import) a CodeWarrior 7.3 .mcp project to convert it. However, it runs into 'Error: unsupported settings panel version in sdm pROM-xRAM'. See attached. Any ideas?

 

149815_149815.pngpastedImage_1.png

Thanks

 

Michael Mojadad

Labels (1)
0 Kudos
1 Reply

245 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Michael

Could you please first open and build your project in CodeWarrior v8.3? CodeWarrior v8.3 can be downloaded from:

CodeWarrior Development Tools for 56800/E DSC|NXP

After it can be working successfully on CW 8.3, import the CW 8.3 project into Eclipse CodeWarrior v10.6.4.

For how to do it, please refer to section 2.8 in CW10.6.4 Targeting Manual:

C:\Freescale\CW MCU v10.6\MCU\Help\PDF\Targeting_Microcontrollers.pdf

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos