AnsweredAssumed Answered

PF0100 :  Schematic is SW1ABC Single Phase with F0 OTP configuration

Question asked by koichi sakagami on May 19, 2016
Latest reply on May 25, 2016 by koichi sakagami

Dear community,
We have been developing our product with iMX6Q and PF0100.

 

We designed the PF0100 Schematic for SW1ABC Single Phase.
In this configuration, all phases A, B, and C, are connected together to a single inductor.

 

But we implemented the F0 type PF0100 chip to custom board in the mistake.
The F0 type Pre-programmed OTP configuration is  (SW1AB Single Phase, SW1C Independent Mode).

 

Reluctantly we are debugging as above situation.
The iMX6Q is working without any problems at the moment .

 

[Question]
In case of continuing to use ,Is there any problem occurs?

 

 

Best Regards,
       Koichi Sakagami

Outcomes