INTLVEN for T1040RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

INTLVEN for T1040RDB

508 Views
hv
Contributor II

I found in the P4080RM the ability to interleave SRAM address space by setting CPCSRCR0[INTLVEN] bit.  But the INTLVEN bit is not defined in the T1040RM.  Does that mean I can't interleave SRAM in the T1040?  Thanks!

0 Kudos
2 Replies

396 Views
alexander_yakov
NXP Employee
NXP Employee

Interleaving may be used only if you have two CPC sram memories. In case of P4080 there are two CPC blocks, but in T1040 there is only one CPC block, so there is nothing to interleave with.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

396 Views
hv
Contributor II

Thanks!

0 Kudos