In the datasheet is the supply voltage of MMA6900 and 6901 not definitely mentioned. 3.3V for 6900 and 5V for 6901? or these two value is optional for the both?
Thank you and best regards,
Mi
Hi Mi,
Both accelerometers (MMA6900 and 6901) can work with 3.3V or 5V.
All the characterized specs mentioned in the datasheet were calculated with these two typical voltage supply on both sensors.
Have a great day,
Jose Reyes
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------