Create Bootstream from Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Create Bootstream from Linux

888 Views
markusvalentin
Contributor II

Hi,

i have a custom compiled Linux and i want to encrypt and sign it. I have some questions:

1. Do i need to use Bootlets or can i get an ivt without them?

2. Is there any example .bd file?

kind regards

Markus

Labels (2)
0 Kudos
1 Reply

659 Views
igorpadykov
NXP Employee
NXP Employee

Hi Markus

1. attached Linux Guide p.1-1 shows bootlet definition

2.  can be found in elftosb documentation

IMX_ELFTOSB_TOOL

Snippets, Boot Code, Headers, Monitors, etc. (4)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos