Zigbee - Is there any reason for a router to leave?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zigbee - Is there any reason for a router to leave?

826 Views
freshmango90
Contributor III

I am using Freescale Beekit, and I have a network up and running. At some point, the router leaves. I did not request it to leave the network, so is there any reason for a router to send a leave request?

Many of the scenarios happen when many devices turn on at the same time, but not limited to that. Other times seem random.

1 Reply

634 Views
jc_pacheco
NXP Employee
NXP Employee

Hello freshmango90,

Can you provide more information about the setup?

What demo are you using?

Do you see this issue on a default demo or did you add some functionality?

How much time does it pass until a router tries to join?

How many devices do you have when this happens?

Under BeeStackConfiguration.h: Did you set gApsMaxSecureMaterialEntries_c and gApsMaxAddrMapEntries_c to be is bigger than the number of devices in the network?

Are you able to replicate this using the latest Kinetis BeeStack ZigBee Protocol Stack (REV 5.0.0) ?

-JC

0 Kudos