AnsweredAssumed Answered

Jtagkey debug JN5168

Question asked by Guillaume Privee on May 11, 2016
Latest reply on Jun 9, 2016 by Bill Krakar

Dear Ms, Mr,

 

I'm developing a project on a JN5168 and I'd like to debug it with the Amontec JtagKey 2 but I have this issue:

(JN-AN-1174 project)

 

 

jp3: JTAG protocol via USB/parallel port for Windows.

Version 1.6.3

Assuming debug_if's TAP has an IDCODE of 0x14951185.

Using 'Amontec Amontec JTAGkey-2 (556XNII6)' interface.

Enabling high speed ftdi mode.

Using JTAG clock of 15 MHz

Enabling UART not supported/required on this adapter.

 

In my makefile, I have:

DEBUG ?=HW

DEBUG_PORT ?= UART0

and TRACE ?=1

 

I respected the application note to start the debug (debug configuration -> _hwdbg.elf ...)

And I also have the transistor on a special pin like this :

P1000880.jpg

 

Can we debug on the JN5168? If yes, what could be my mistake?

 

Thank you!

Outcomes