About the default Interrupt Prioriy of KE06 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the default Interrupt Prioriy of KE06 MCU

557 Views
freei
Contributor I

Where can I find the default interrupt priority of Ke06 MCU ? If I don't change the defalut mode,IRQ12 's priority is higher than IRQ17?

Can I Set IRQ17's priority higher than IRQ12 by setting the NVICIPR4 register?

Thanks!

Labels (1)
0 Kudos
1 Reply

429 Views
pavel_krenek
NXP Employee
NXP Employee

Hello,

default priority of all interrupts on KE06 (ARM cortex M0+ core) are 0, that means the highest possible priority. If you would like to change the priority to higher for IRQ17 you have to change all other used interrupts to lower value that for IRQ17.

Best regards,

Pavel

0 Kudos