Hi,
The images is come from nxp official website that name is android_L5.1.1_2.1.0_core_image_6dqsabresd and android_KK4.4.3_2.0.0-ga_core_image_6qsabresd.
Development board is MCIMX6Q-SDB.
Msgtool is IMX6_L5.1_2.1.0_MFG_TOOL.tar.gz.
I was download images by mfgtool2-android-mx6q-sabresd-sd.vbs, but the mfgtool will stop and display "No device connected " after "Jumping to OS image" , I will upload the uart log during this period. Can you help me trace the problem?
Thanks.
Original Attachment has been moved to: log.zip
Hi ferdinand yang,
Sorry for late reply, I do not know if your board can run successfully. About downloading with mfgtool you can refer to Android_Quick_Start_Guide.pdf document, details are in it. You also can have a try to download the images to emmc.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
The original system of the board can be normal operation, but I don't know the version of Android, because I don't have touch screen.
I had try to download images to emmc but also failed ,you can see the attachment of log.
Thanks.