Axel Hubner

S12ZVH128 CPU Frequency

Discussion created by Axel Hubner on May 9, 2016
Latest reply on May 11, 2016 by Axel Hubner

Hi,

 

i am currently using the TRK S12ZVH128 evolution board for pre-development.

I am trying to set the CPU Bus frequency up to 32Mhz (Max frequency).

Unfortunately the code always crashes when I try to set the CPMUSYNR register.

To eliminate bugs on my code i also tried to generate the CPU init code with processor expert, but it still crashes.

When i reduce the frequency down to 26 Mhz the initialization seems to work.

As i told, we are using the S12ZVH128 for pre-developing. For the product itself a S12zVH64 is planned.

If i run the code with the S12zVH64 it seems to work correctly. Why can't i use the maximum frequency for the S12ZVH128 and is it a problem to use 32Mhz for the S12zVH64?

 

 

void _EntryPoint(void)

{

  /*** !!! Here you can place your own code using property "User code before PE initialization" on the build options tab of the CPU compoennt. !!! ***/

  /* ### MC9S12ZVH128_144 "Cpu" init code ... */

  /*  PE initialization code after reset */

  /* IVBR: IVB_ADDR=0x7FFF,??=0 */

  setReg16(IVBR, 0xFFFEU);             

  /* ECLKCTL: NECLK=1,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  setReg8(ECLKCTL, 0x80U);             

  /*  System clock initialization */

  /* CPMUPROT: ??=0,??=0,??=1,??=0,??=0,??=1,??=1,PROT=0 */

  setReg8(CPMUPROT, 0x26U);            /* Disable protection of clock configuration registers */

  /* CPMUCLKS: PSTP=0 */

  clrReg8Bits(CPMUCLKS, 0x40U);        

  /* CPMUCLKS: PLLSEL=1 */

  setReg8Bits(CPMUCLKS, 0x80U);        /* Enable the PLL to allow write to divider registers */

  /* CPMUPOSTDIV: ??=0,??=0,??=0,POSTDIV4=0,POSTDIV3=0,POSTDIV2=0,POSTDIV1=0,POSTDIV0=0 */

  setReg8(CPMUPOSTDIV, 0x00U);         /* Set the post divider register */

  /* Whenever changing PLL reference clock (REFCLK) frequency to a higher value

   it is recommended to write CPMUSYNR = 0x00 in order to stay within specified

   maximum frequency of the MCU */

  /* CPMUSYNR: VCOFRQ1=0,VCOFRQ0=0,SYNDIV5=0,SYNDIV4=0,SYNDIV3=0,SYNDIV2=0,SYNDIV1=0,SYNDIV0=0 */

  setReg8(CPMUSYNR, 0x00U);            /* Set the multiplier register */

  /* CPMUPLL: ??=0,??=0,FM1=0,FM0=0,??=0,??=0,??=0,??=0 */

  setReg8(CPMUPLL, 0x00U);             /* Set the PLL frequency modulation */

  /* CPMUSYNR: VCOFRQ1=0,VCOFRQ0=1,SYNDIV5=0,SYNDIV4=1,SYNDIV3=1,SYNDIV2=1,SYNDIV1=1,SYNDIV0=1 */

  setReg8(CPMUSYNR, 0x5FU);            /* Set the multiplier register */  --> Crash

 

Regards

Axel

Outcomes