hello experts
i have a P2020 board
to save coset i will plan to use P1011 with the same board
to test program i will like to replace P2020 cpu with P1011 cpu
but the board have Core0, Core1 power Pin connected to Power which can not be disconnected
in P1011 datasheet those pins are "NC"
i just double-check it's OK to connect those pins with Power
thank you
Yes, core1 power supply VDD is allowed to be connected to core0/platform power supply VDDC. The following is said in Design Checklist: "In single core devices, VDD can be connected to GND to save power, or else VDD should be connected from VDDC"
Here is a direct link to P1020/P1011 design checklist (application note AN4259):
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------