Hello Champs,
In LTIB verson of u-boot, ipu1_clk is set 260MHz in default.
However in the Yocto u-boot, it is defined as 198MHz.
#ifdef CONFIG_MX6DL |
#define CONFIG_IPUV3_CLK 198000000
#else
#define CONFIG_IPUV3_CLK 264000000
#endif
Is this because ipu_clk was turned out actually limited to 198MHz in MX6DL?
Or just because a result of clock tree changes in Yocto u-boot?
BR,
N.S.
Hi Nori
you are right: this seems as result of clock tree changes,
max. frequency is described in Table 18-4. System Clock Frequency Values
i.MX6SDL Reference Manual
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------