I want to set up the WiFi and Bluetooth(WL1835) on our custom board, where also it is connected to SD2 interface(WiFi) and UART2(BT). Now my question is I have drivers in the kernel 3.14.28 for wlcore, wl18xx and bluetooth ,will this driver code will work or I need to modify something?
If I need to modify then what part of the driver I need to modify?
Do I need to make changes in Device tree ?
Can I access the WiFi at u-Boot level, if yes then How?
What changes I need to do in the Device Tree File ?
If you have any sample device tree file with related changes , plz. share with me.
Thank You.
one can follow 3.10.53 bring-up steps
Step-by-step: How to setup TI Wilink (WL18xx) with iMX6 Linux 3.10.53
Best regards
igor
Thanks for Reply.
They have given the description for 2.6 kernel but
I want to set up in 3.14.28
On Fri, May 6, 2016 at 4:21 PM, igorpadykov <admin@community.freescale.com>
But After that it requires to apply patches and I don't know which patches to apply?
Hello,
TI has the wiki page for integration with i.MX
http://processors.wiki.ti.com/index.php/WL18xx_First_Time_Getting_Started_Guide_(IMX6)
Luis
Thanks for Reply.
I have that modules with me but I just want to know do I need to modify the driver codes?
because while traversing driver code I am unable to find pin related info