Hi,
There are some documentation about MQX in k50n512 integrated with HTTP and SNMP?
Thank you.
Best Regards
Flavio
Hello Flavio,
After install MQX you can find some example application at the next path; you can use these examples as reference,
C:\Freescale\Freescale_MQX_4_2\rtcs\examples
eth_to_serial: Simple character passing between the UART console and the telnet session. Shows custom "lightweight" telnet.
Httpsrv: Simple web server with CGI-like scripts and web pages stored in internal flash.
Shell: Shell command line providing commands for network management.
Snmp: SNMP protocol example providing microprocessor state information.
For HTTP, in the following links you can find more example applications:
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4417.pdf
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4345.pdf
http://cache.nxp.com/files/32bit/doc/app_note/AN4022.pdf
Unfortunately we don’t have an example implementing HTTP and SNMP.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------